PlantOutputCollection Class¶
-
class
NXOpen.Motion.
PlantOutputCollection
¶ Bases:
object
Represents a collection of Plant Output objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreatePlantOutputBuilder | Creates a NXOpen.Motion.PlantOutputBuilder @return |
FindObject | Finds the NXOpen.Motion.PlantOutput with the given name. |
Method Detail¶
CreatePlantOutputBuilder¶
-
PlantOutputCollection.
CreatePlantOutputBuilder
¶ Creates a
NXOpen.Motion.PlantOutputBuilder
Signature
CreatePlantOutputBuilder(platoutput)
Parameters: platoutput ( NXOpen.Motion.PlantOutput
) –Returns: Return type: NXOpen.Motion.PlantOutputBuilder
New in version NX6.0.0.
License requirements: nx_motion_cosim (“NX Motion CoSimulation”)
FindObject¶
-
PlantOutputCollection.
FindObject
¶ Finds the
NXOpen.Motion.PlantOutput
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.PlantOutput
.Returns: NXOpen.Motion.PlantOutput
with this name.Return type: NXOpen.Motion.PlantOutput
New in version NX6.0.0.
License requirements: nx_motion_cosim (“NX Motion CoSimulation”)