PackagingTraceBuilder Class¶
-
class
NXOpen.Motion.
PackagingTraceBuilder
¶ Bases:
NXOpen.Motion.PackagingBuilder
This is the builder class to create or edit a Trace object.
To create a new instance of this class, use
NXOpen.Motion.PackagingCollection.CreateTraceBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Enable | Returns or sets the enable flag of NXOpen.Motion.Packaging object. |
FrameType | Returns or sets the NXOpen.Motion.PackagingTrace reference frame type defined at NXOpen.Motion.PackagingTraceBuilderFrame |
Name | Returns or sets the name of NXOpen.Motion.Packaging object. |
Tag | Returns the Tag for this object. |
TargetLayer | Returns or sets the NXOpen.Motion.PackagingTrace target layer |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetList1 | Returns geometry list 1 of NXOpen.Motion.Packaging object. |
GetObject | Returns the object currently being edited by this builder. |
GetRelativeLinks | Returns NXOpen.Motion.PackagingTrace relative links. |
SetList1 | Sets geometry list 1. |
SetRelativeLinks | Sets NXOpen.Motion.PackagingTrace relative links. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PackagingTraceBuilderFrame Enumeration | Trace reference frame type |
Property Detail¶
FrameType¶
-
PackagingTraceBuilder.
FrameType
¶ Returns or sets the
NXOpen.Motion.PackagingTrace
reference frame type defined atNXOpen.Motion.PackagingTraceBuilderFrame
-------------------------------------
Getter Method
Signature
FrameType()
Returns: Trace reference frame type defined in NXOpen.Motion.PackagingTraceBuilderFrame
:rtype:NXOpen.Motion.PackagingTraceBuilderFrame
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
FrameType(fType)
Parameters: fType ( NXOpen.Motion.PackagingTraceBuilderFrame
) – Trace reference frame type defined inNXOpen.Motion.PackagingTraceBuilderFrame
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
TargetLayer¶
-
PackagingTraceBuilder.
TargetLayer
¶ Returns or sets the
NXOpen.Motion.PackagingTrace
target layer-------------------------------------
Getter Method
Signature
TargetLayer()
Returns: Target layer Return type: int New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
TargetLayer(targetLayer)
Parameters: targetLayer (int) – Target layer New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
GetRelativeLinks¶
-
PackagingTraceBuilder.
GetRelativeLinks
¶ Returns
NXOpen.Motion.PackagingTrace
relative links.Only available when frame type is :py:class:` NXOpen.Motion.PackagingTraceBuilderFrame.Relative < NXOpen.Motion.PackagingTraceBuilderFrame>`.
Signature
GetRelativeLinks()
Returns: The list pointer Return type: list of NXOpen.DisplayableObject
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetRelativeLinks¶
-
PackagingTraceBuilder.
SetRelativeLinks
¶ Sets
NXOpen.Motion.PackagingTrace
relative links.Only used when frame type is :py:class:` NXOpen.Motion.PackagingTraceBuilderFrame.Relative < NXOpen.Motion.PackagingTraceBuilderFrame>`.
Signature
SetRelativeLinks(links)
Parameters: links (list of NXOpen.DisplayableObject
) – The list pointerNew in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
Validate¶
-
PackagingTraceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.