PackagingMeasureBuilderMeasureCondition Enumeration¶
NXOpen.Motion.PackagingMeasureBuilder.MeasureCondition is an alias for NXOpen.Motion.PackagingMeasureBuilderMeasureCondition
-
class
NXOpen.Motion.
PackagingMeasureBuilderMeasureCondition
¶ Bases:
object
Measure condition
Enum Members
- less than threshold value. “
- “GreaterThan”, ” Stop event defined by minimum measurement
- greater than threshold value. “
- “EqualTo”, ” Stop event defined by minimum measurement
equal to threshold (target) value. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.