PackagingInterferenceBuilderFrame Enumeration¶
NXOpen.Motion.PackagingInterferenceBuilder.Frame is an alias for NXOpen.Motion.PackagingInterferenceBuilderFrame
-
class
NXOpen.Motion.
PackagingInterferenceBuilderFrame
¶ Bases:
object
Interference solid reference frame type.
Only used for action type of :py:class:` NXOpen.Motion.PackagingInterferenceBuilderAction.CreateSolids < NXOpen.Motion.PackagingInterferenceBuilderAction>`.
Enum Members
- coordinate system. “
- “FirstSet”, ” Interference solids positioned relative to
- interfering links in first set. “
- “SecondSet”, ” Interference solids positioned relative to
- interfering links in second set. “
- “BothSets”, ” Interference solids positioned relative to
- interfering links in both sets. “
- “Selected”, ” Interference solids positioned relative to
user selected links. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.