PMDCMotorCollection Class¶
-
class
NXOpen.Motion.
PMDCMotorCollection
¶ Bases:
object
Represents a collection of motion pmdc motor
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreatePmdcMotorBuilder | Return NXOpen.Motion.PMDCMotorBuilder object @return PMDCMotorBuilder object |
FindObject | Finds the NXOpen.Motion.PMDCMotor with the given name. |
Method Detail¶
CreatePmdcMotorBuilder¶
-
PMDCMotorCollection.
CreatePmdcMotorBuilder
¶ Return
NXOpen.Motion.PMDCMotorBuilder
objectSignature
CreatePmdcMotorBuilder(pmdcMotor)
Parameters: pmdcMotor ( NXOpen.Motion.PMDCMotor
) –NXOpen.Motion.PMDCMotor
to be edited, if None then create a new oneReturns: PMDCMotorBuilder object Return type: NXOpen.Motion.PMDCMotorBuilder
New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
FindObject¶
-
PMDCMotorCollection.
FindObject
¶ Finds the
NXOpen.Motion.PMDCMotor
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.Motion.PMDCMotor
New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)