MotionMethods Class¶
-
class
NXOpen.Motion.
MotionMethods
¶ Bases:
object
Represents a
NXOpen.Motion.MotionMethods
classTo obtain an instance of this class, refer to
NXOpen.Motion.MotionSession
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CopyConnectorParameters | Copies the connector parameters |
ModelCheck | Check all motion objects |
Method Detail¶
CopyConnectorParameters¶
-
MotionMethods.
CopyConnectorParameters
¶ Copies the connector parameters
Signature
CopyConnectorParameters(sourceConnector, destinationConnector)
Parameters: - sourceConnector (
NXOpen.NXObject
) – Source connector from which parameters are copied - destinationConnector (
NXOpen.NXObject
) – Destination connector to which the paramaters are copied
New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
- sourceConnector (