MarkerMarkerType Enumeration¶
NXOpen.Motion.Marker.MarkerType is an alias for NXOpen.Motion.MarkerMarkerType
-
class
NXOpen.Motion.
MarkerMarkerType
¶ Bases:
object
Marker subtype
Enum Members
- It will be automatically created for a link. “
- “UserDefined”, ” User created marker. It can be attached to any motion object. ” “CenterOfMass”, ” Defines the center of mass for a link.
It will be automatically created for a link. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.