LinkInitialVelocityAngularVelocityType Enumeration¶
NXOpen.Motion.LinkInitialVelocity.AngularVelocityType is an alias for NXOpen.Motion.LinkInitialVelocityAngularVelocityType
-
class
NXOpen.Motion.
LinkInitialVelocityAngularVelocityType
¶ Bases:
object
Defines rotate type of initial velocity.
If
NXOpen.Motion.LinkInitialVelocityAngularVelocityType.Magnitude
is set,NXOpen.Motion.LinkInitialVelocity.RotateVector()
andNXOpen.Motion.LinkInitialVelocity.RotateMagnitude()
is valid.IfNXOpen.Motion.LinkInitialVelocityAngularVelocityType.Component
is selected,NXOpen.Motion.LinkInitialVelocity.RotateCsys()
,NXOpen.Motion.LinkInitialVelocity.Wx()
,NXOpen.Motion.LinkInitialVelocity.Wy()
, andNXOpen.Motion.LinkInitialVelocity.Wz()
is valid.Enum Members
Enum Member Enum Member Description Magnitude Magnitude type define rotate vectorComponent Component type define rotate csys-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-