LinkCollection Class¶
-
class
NXOpen.Motion.
LinkCollection
¶ Bases:
object
Represents a collection of motion joints
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateFixedJoint | Creates a NXOpen.Motion.Joint @return |
CreateLinkBuilder | Creates a NXOpen.Motion.LinkBuilder @return |
FindObject | Finds the NXOpen.Motion.Link with the given name. |
Method Detail¶
CreateFixedJoint¶
-
LinkCollection.
CreateFixedJoint
¶ Creates a
NXOpen.Motion.Joint
Signature
CreateFixedJoint(link)
Parameters: link ( NXOpen.Motion.Link
) –NXOpen.Motion.Link
to be used to create relate fixed jointReturns: Return type: NXOpen.Motion.Joint
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
CreateLinkBuilder¶
-
LinkCollection.
CreateLinkBuilder
¶ Creates a
NXOpen.Motion.LinkBuilder
Signature
CreateLinkBuilder(link)
Parameters: link ( NXOpen.Motion.Link
) –NXOpen.Motion.Link
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.LinkBuilder
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
LinkCollection.
FindObject
¶ Finds the
NXOpen.Motion.Link
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.Link
.Returns: NXOpen.Motion.Link
with this name.Return type: NXOpen.Motion.Link
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)