GraphBuilderComponentChoices Enumeration¶
NXOpen.Motion.GraphBuilder.ComponentChoices is an alias for NXOpen.Motion.GraphBuilderComponentChoices
-
class
NXOpen.Motion.
GraphBuilderComponentChoices
¶ Bases:
object
Component attribute of the curve data.
Enum Members
Enum Member Enum Member Description Mag MagnitudeX XY YZ ZAmag Angular MagnitudeXy XYYz YZZx ZXInputVoltage Input VoltageElectricCurrent Electric CurrentElectricTorque Electric TorqueSignalChart Signal Chart-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-