GeneralCouplerCollection Class¶
-
class
NXOpen.Motion.
GeneralCouplerCollection
¶ Bases:
object
Represents a collection of 2-3 joint coupler objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreateGeneralCouplerBuilder | Creates a NXOpen.Motion.GeneralCouplerBuilder @return |
FindObject | Finds the NXOpen.Motion.GeneralCoupler with the given name. |
Method Detail¶
CreateGeneralCouplerBuilder¶
-
GeneralCouplerCollection.
CreateGeneralCouplerBuilder
¶ Creates a
NXOpen.Motion.GeneralCouplerBuilder
Signature
CreateGeneralCouplerBuilder(gcoupler)
Parameters: gcoupler ( NXOpen.Motion.GeneralCoupler
) –Returns: Return type: NXOpen.Motion.GeneralCouplerBuilder
New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
GeneralCouplerCollection.
FindObject
¶ Finds the
NXOpen.Motion.GeneralCoupler
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.GeneralCoupler
.Returns: NXOpen.Motion.GeneralCoupler
with this name.Return type: NXOpen.Motion.GeneralCoupler
New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)