DriverOperationType Enumeration¶
NXOpen.Motion.DriverOperation.Type is an alias for NXOpen.Motion.DriverOperationType
-
class
NXOpen.Motion.
DriverOperationType
¶ Bases:
object
Driver operation type
Enum Members
Enum Member Enum Member Description Undefined UndefinedConstant Constant; Deprecated in NX11.0; use type_polynomial insteadPolynomial PolynomialHarmonic HarmonicFunction FunctionArticulation ArticulationMotor MotorControl Control-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-