DriverMotionsDataDriverRotationType Enumeration¶
NXOpen.Motion.DriverMotionsData.DriverRotationType is an alias for NXOpen.Motion.DriverMotionsDataDriverRotationType
-
class
NXOpen.Motion.
DriverMotionsDataDriverRotationType
¶ Bases:
object
Driver Rotation type
Enum Members
Enum Member Enum Member Description Successive Rotations are applied to the rotated link (as defined by previous rotations)Fixed Rotations are applied to the original position of the link-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-