CurveOnCurveCollection Class¶
-
class
NXOpen.Motion.
CurveOnCurveCollection
¶ Bases:
object
Represents a collection of curve on curve objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateCurveOnCurveBuilder | Creates a NXOpen.Motion.CurveOnCurveBuilder @return |
FindObject | Finds the NXOpen.Motion.CurveOnCurve with the given name. |
Method Detail¶
CreateCurveOnCurveBuilder¶
-
CurveOnCurveCollection.
CreateCurveOnCurveBuilder
¶ Creates a
NXOpen.Motion.CurveOnCurveBuilder
Signature
CreateCurveOnCurveBuilder(curveOnCurve)
Parameters: curveOnCurve ( NXOpen.Motion.CurveOnCurve
) –NXOpen.Motion.CurveOnCurve
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.CurveOnCurveBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
CurveOnCurveCollection.
FindObject
¶ Finds the
NXOpen.Motion.CurveOnCurve
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.CurveOnCurve
.Returns: NXOpen.Motion.CurveOnCurve
with this name.Return type: NXOpen.Motion.CurveOnCurve
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)