CurveContactCollection Class¶
-
class
NXOpen.Motion.
CurveContactCollection
¶ Bases:
object
Represents a collection of 2D contact objects.
Any 2D contact object must be created and found through this class To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateCurveContactBuilder | Creates a NXOpen.Motion.CurveContact @return |
FindObject | Finds the NXOpen.Motion.CurveContact with the given name. |
Method Detail¶
CreateCurveContactBuilder¶
-
CurveContactCollection.
CreateCurveContactBuilder
¶ Creates a
NXOpen.Motion.CurveContact
Signature
CreateCurveContactBuilder(contactobj)
Parameters: contactobj ( NXOpen.Motion.CurveContact
) – “NXOpen.Motion.CurveContact
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.CurveContactBuilder
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
CurveContactCollection.
FindObject
¶ Finds the
NXOpen.Motion.CurveContact
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.CurveContact
.Returns: NXOpen.Motion.CurveContact
with this name.Return type: NXOpen.Motion.CurveContact
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)