CouplerCollection Class¶
-
class
NXOpen.Motion.
CouplerCollection
¶ Bases:
object
Represents a collection of motion couplers
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateCouplerCableBuilder | Creates the builder object of NXOpen.Motion.CouplerCable object @return |
CreateCouplerGearBuilder | Creates the builder object of NXOpen.Motion.CouplerGear object @return |
CreateCouplerRckpnBuilder | Creates the builder object of NXOpen.Motion.CouplerRckpn object @return |
FindObject | Finds a coupler with the given name. |
Method Detail¶
CreateCouplerCableBuilder¶
-
CouplerCollection.
CreateCouplerCableBuilder
¶ Creates the builder object of
NXOpen.Motion.CouplerCable
objectSignature
CreateCouplerCableBuilder(coupler)
Parameters: coupler ( NXOpen.Motion.CouplerCable
) –Returns: Return type: NXOpen.Motion.CouplerCableBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
CreateCouplerGearBuilder¶
-
CouplerCollection.
CreateCouplerGearBuilder
¶ Creates the builder object of
NXOpen.Motion.CouplerGear
objectSignature
CreateCouplerGearBuilder(coupler)
Parameters: coupler ( NXOpen.Motion.CouplerGear
) –Returns: Return type: NXOpen.Motion.CouplerGearBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
CreateCouplerRckpnBuilder¶
-
CouplerCollection.
CreateCouplerRckpnBuilder
¶ Creates the builder object of
NXOpen.Motion.CouplerRckpn
objectSignature
CreateCouplerRckpnBuilder(coupler)
Parameters: coupler ( NXOpen.Motion.CouplerRckpn
) –Returns: Return type: NXOpen.Motion.CouplerRckpnBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
CouplerCollection.
FindObject
¶ Finds a coupler with the given name.
An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the Motion.Coupler
.Returns: Motion.Coupler
with this name.Return type: NXOpen.Motion.Coupler
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)