ControlOutputBuilderControlOutputType Enumeration¶
NXOpen.Motion.ControlOutputBuilder.ControlOutputType is an alias for NXOpen.Motion.ControlOutputBuilderControlOutputType
-
class
NXOpen.Motion.
ControlOutputBuilderControlOutputType
¶ Bases:
object
Control Output type
Enum Members
Enum Member Enum Member Description Link Control Output Type Link. Requires an action link attachment. Can have a base link attachment.JointOrConstraint Control Output Type Joint or Constraint. Requires a Joint or Point on Curve Constraint as input.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-