ControlInputPortBuilderMeasuredComponent Enumeration¶
NXOpen.Motion.ControlInputPortBuilder.MeasuredComponent is an alias for NXOpen.Motion.ControlInputPortBuilderMeasuredComponent
-
class
NXOpen.Motion.
ControlInputPortBuilderMeasuredComponent
¶ Bases:
object
the types of components that can be measured by the control input element for the selected variable.
Enum Members
Enum Member Enum Member Description LinearMagnitude Linear MagnitudeX XY YZ ZAngularMagnitude Angular MagnitudeRx RXRy RYRz RZ-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-