ConfigurationParameter Class

class NXOpen.Motion.ConfigurationParameter

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a Motion.ConfigurationParameter.

This class contains the port association for the output of a mechatronics element No KF support

New in version NX11.0.0.

Properties

Property Description
Name Returns the name
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Name

ConfigurationParameter.Name

Returns the name

-------------------------------------

Getter Method

Signature Name()

Returns:
Return type:str

New in version NX11.0.0.

License requirements: mechanisms (“MECHANISMS”)

Method Detail

Validate

ConfigurationParameter.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.