BushingCylindricalCoefficientsComponent Class¶
-
class
NXOpen.Motion.
BushingCylindricalCoefficientsComponent
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Motion BushingCylindricalCoefficientsComponent
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Conical | Returns or sets the conical coefficient, it is available only when Motion.BushingCylindricalCoefficientsComponent.ConicalType`() set to MotionConnectorCoefficientTypes.Constant case |
ConicalExpression | Returns the conical coefficient expression, it is available only when Motion.BushingCylindricalCoefficientsComponent.ConicalType`() set to MotionConnectorCoefficientTypes.Constant case |
ConicalFunction | Returns or sets the conical function tag, it is available only when Motion.BushingCylindricalCoefficientsComponent.ConicalType`() set to MotionConnectorCoefficientTypes.Spline case |
ConicalType | Returns or sets the conical coefficient type |
Longitudinal | Returns or sets the longitudinal double value, it is available only when Motion.BushingCylindricalCoefficientsComponent.RadialType`() set to MotionConnectorCoefficientTypes.Constant case |
LongitudinalExpression | Returns the longitudinal coefficient expression, it is available only when Motion.BushingCylindricalCoefficientsComponent.RadialType`() set to MotionConnectorCoefficientTypes.Constant case |
LongitudinalFunction | Returns or sets the longitudinal function tag, it is available only when Motion.BushingCylindricalCoefficientsComponent.RadialType`() set to MotionConnectorCoefficientTypes.Spline case |
Radial | Returns or sets the radial, it is available only when Motion.BushingCylindricalCoefficientsComponent.RadialType`() set to MotionConnectorCoefficientTypes.Constant case |
RadialExpression | Returns the radial coefficient expression, it is available only when Motion.BushingCylindricalCoefficientsComponent.RadialType`() set to MotionConnectorCoefficientTypes.Constant case |
RadialFunction | Returns or sets the radial function tag, it is available only when Motion.BushingCylindricalCoefficientsComponent.RadialType`() set to MotionConnectorCoefficientTypes.Spline case |
RadialType | Returns or sets the radial type |
Tag | Returns the Tag for this object. |
Torsional | Returns or sets the torsional coefficient, it is available only when Motion.BushingCylindricalCoefficientsComponent.ConicalType`() set to MotionConnectorCoefficientTypes.Constant case |
TorsionalExpression | Returns the torsional coefficient expression, it is available only when Motion.BushingCylindricalCoefficientsComponent.ConicalType`() set to MotionConnectorCoefficientTypes.Constant case |
TorsionalFunction | Returns or sets the torsional function tag, it is available only when Motion.BushingCylindricalCoefficientsComponent.ConicalType`() set to MotionConnectorCoefficientTypes.Spline case |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Conical¶
-
BushingCylindricalCoefficientsComponent.
Conical
¶ Returns or sets the conical coefficient, it is available only when
Motion.BushingCylindricalCoefficientsComponent.ConicalType`()
set toMotionConnectorCoefficientTypes.Constant
case-------------------------------------
Getter Method
Signature
Conical()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
Motion.BushingCylindricalCoefficientsComponent.ConicalExpression()
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
Conical(conical)
Parameters: conical (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
Motion.BushingCylindricalCoefficientsComponent.ConicalExpression()
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
ConicalExpression¶
-
BushingCylindricalCoefficientsComponent.
ConicalExpression
¶ Returns the conical coefficient expression, it is available only when
Motion.BushingCylindricalCoefficientsComponent.ConicalType`()
set toMotionConnectorCoefficientTypes.Constant
case-------------------------------------
Getter Method
Signature
ConicalExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ConicalFunction¶
-
BushingCylindricalCoefficientsComponent.
ConicalFunction
¶ Returns or sets the conical function tag, it is available only when
Motion.BushingCylindricalCoefficientsComponent.ConicalType`()
set toMotionConnectorCoefficientTypes.Spline
case-------------------------------------
Getter Method
Signature
ConicalFunction()
Returns: Return type: NXOpen.CAE.Function
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConicalFunction(function)
Parameters: function ( NXOpen.CAE.Function
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
ConicalType¶
-
BushingCylindricalCoefficientsComponent.
ConicalType
¶ Returns or sets the conical coefficient type
-------------------------------------
Getter Method
Signature
ConicalType()
Returns: Return type: NXOpen.Motion.ConnectorCoefficientTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConicalType(conicalType)
Parameters: conicalType ( NXOpen.Motion.ConnectorCoefficientTypes
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Longitudinal¶
-
BushingCylindricalCoefficientsComponent.
Longitudinal
¶ Returns or sets the longitudinal double value, it is available only when
Motion.BushingCylindricalCoefficientsComponent.RadialType`()
set toMotionConnectorCoefficientTypes.Constant
case-------------------------------------
Getter Method
Signature
Longitudinal()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
Motion.BushingCylindricalCoefficientsComponent.LongitudinalExpression()
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
Longitudinal(longitudinal)
Parameters: longitudinal (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
Motion.BushingCylindricalCoefficientsComponent.LongitudinalExpression()
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
LongitudinalExpression¶
-
BushingCylindricalCoefficientsComponent.
LongitudinalExpression
¶ Returns the longitudinal coefficient expression, it is available only when
Motion.BushingCylindricalCoefficientsComponent.RadialType`()
set toMotionConnectorCoefficientTypes.Constant
case-------------------------------------
Getter Method
Signature
LongitudinalExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
LongitudinalFunction¶
-
BushingCylindricalCoefficientsComponent.
LongitudinalFunction
¶ Returns or sets the longitudinal function tag, it is available only when
Motion.BushingCylindricalCoefficientsComponent.RadialType`()
set toMotionConnectorCoefficientTypes.Spline
case-------------------------------------
Getter Method
Signature
LongitudinalFunction()
Returns: Return type: NXOpen.CAE.Function
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LongitudinalFunction(function)
Parameters: function ( NXOpen.CAE.Function
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Radial¶
-
BushingCylindricalCoefficientsComponent.
Radial
¶ Returns or sets the radial, it is available only when
Motion.BushingCylindricalCoefficientsComponent.RadialType`()
set toMotionConnectorCoefficientTypes.Constant
case-------------------------------------
Getter Method
Signature
Radial()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
Motion.BushingCylindricalCoefficientsComponent.RadialExpression()
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
Radial(radial)
Parameters: radial (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
Motion.BushingCylindricalCoefficientsComponent.RadialExpression()
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
RadialExpression¶
-
BushingCylindricalCoefficientsComponent.
RadialExpression
¶ Returns the radial coefficient expression, it is available only when
Motion.BushingCylindricalCoefficientsComponent.RadialType`()
set toMotionConnectorCoefficientTypes.Constant
case-------------------------------------
Getter Method
Signature
RadialExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
RadialFunction¶
-
BushingCylindricalCoefficientsComponent.
RadialFunction
¶ Returns or sets the radial function tag, it is available only when
Motion.BushingCylindricalCoefficientsComponent.RadialType`()
set toMotionConnectorCoefficientTypes.Spline
case-------------------------------------
Getter Method
Signature
RadialFunction()
Returns: Return type: NXOpen.CAE.Function
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialFunction(function)
Parameters: function ( NXOpen.CAE.Function
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
RadialType¶
-
BushingCylindricalCoefficientsComponent.
RadialType
¶ Returns or sets the radial type
-------------------------------------
Getter Method
Signature
RadialType()
Returns: Return type: NXOpen.Motion.ConnectorCoefficientTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialType(radialType)
Parameters: radialType ( NXOpen.Motion.ConnectorCoefficientTypes
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Torsional¶
-
BushingCylindricalCoefficientsComponent.
Torsional
¶ Returns or sets the torsional coefficient, it is available only when
Motion.BushingCylindricalCoefficientsComponent.ConicalType`()
set toMotionConnectorCoefficientTypes.Constant
case-------------------------------------
Getter Method
Signature
Torsional()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
Motion.BushingCylindricalCoefficientsComponent.TorsionalExpression()
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
Torsional(torsional)
Parameters: torsional (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
Motion.BushingCylindricalCoefficientsComponent.TorsionalExpression()
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
TorsionalExpression¶
-
BushingCylindricalCoefficientsComponent.
TorsionalExpression
¶ Returns the torsional coefficient expression, it is available only when
Motion.BushingCylindricalCoefficientsComponent.ConicalType`()
set toMotionConnectorCoefficientTypes.Constant
case-------------------------------------
Getter Method
Signature
TorsionalExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
TorsionalFunction¶
-
BushingCylindricalCoefficientsComponent.
TorsionalFunction
¶ Returns or sets the torsional function tag, it is available only when
Motion.BushingCylindricalCoefficientsComponent.ConicalType`()
set toMotionConnectorCoefficientTypes.Spline
case-------------------------------------
Getter Method
Signature
TorsionalFunction()
Returns: Return type: NXOpen.CAE.Function
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TorsionalFunction(function)
Parameters: function ( NXOpen.CAE.Function
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
BushingCylindricalCoefficientsComponent.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.