BushingCollection Class¶
-
class
NXOpen.Motion.
BushingCollection
¶ Bases:
object
Represents a collection of motion joints
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateBushingBuilder | Return NXOpen.Motion.BushingBuilder object @return BushingBuilder object |
FindObject | Finds the NXOpen.Motion.Bushing with the given name. |
Method Detail¶
CreateBushingBuilder¶
-
BushingCollection.
CreateBushingBuilder
¶ Return
NXOpen.Motion.BushingBuilder
objectSignature
CreateBushingBuilder(bushing)
Parameters: bushing ( NXOpen.Motion.Bushing
) –NXOpen.Motion.Bushing
to be edited, if None then create a new oneReturns: BushingBuilder object Return type: NXOpen.Motion.BushingBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
BushingCollection.
FindObject
¶ Finds the
NXOpen.Motion.Bushing
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.Bushing
.Returns: NXOpen.Motion.Bushing
with this name.Return type: NXOpen.Motion.Bushing
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)