Properties¶
Property | Description |
---|---|
EntryType | Returns the type of this menu entry. |
IsDefault | Returns true if this entry is the default action for the menu. |
IsHidden | Returns true if this entry is hidden on the menu. |
IsSensitive | Returns true if the command corresponding to this entry can be run. |
Label | Returns the label of this menu entry. |
Name | Returns the name of this menu entry. |
Enumerations¶
ContextMenuEntryType Enumeration | Specifies the type of the menu entry. |
Property Detail¶
EntryType¶
-
ContextMenuEntry.
EntryType
¶ Returns the type of this menu entry.
-------------------------------------
Getter Method
Signature
EntryType()
Returns: Return type: NXOpen.MenuBar.ContextMenuEntryType
New in version NX8.5.0.
License requirements: None.
IsDefault¶
-
ContextMenuEntry.
IsDefault
¶ Returns true if this entry is the default action for the menu.
A menu entry is marked as the default for the menu when it corresponds to the double-click action.
-------------------------------------
Getter Method
Signature
IsDefault()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
IsSensitive¶
-
ContextMenuEntry.
IsSensitive
¶ Returns true if the command corresponding to this entry can be run.
-------------------------------------
Getter Method
Signature
IsSensitive()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
Label¶
-
ContextMenuEntry.
Label
¶ Returns the label of this menu entry.
-------------------------------------
Getter Method
Signature
Label()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
Name¶
-
ContextMenuEntry.
Name
¶ Returns the name of this menu entry.
Some entries on the context menu may correspond to buttons on the menu bar. For these entries, the name that is returned is the name of that
MenuBar.MenuButton
object.For all other entries which do not correspond to a menu bar button, the name that is returned has no specific meaning. However, for any individual action within any specific context menu, the name that is assigned to that action will not change.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.