SystemObjectReorderType Enumeration

NXOpen.Mechatronics.SystemObject.ReorderType is an alias for NXOpen.Mechatronics.SystemObjectReorderType

class NXOpen.Mechatronics.SystemObjectReorderType

Bases: object

Reorder object type to specify the relative position.

Enum Members

Enum Member Enum Member Description
Before
Before
After
After
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.