SystemObjectRelationType Enumeration

NXOpen.Mechatronics.SystemObject.RelationType is an alias for NXOpen.Mechatronics.SystemObjectRelationType

class NXOpen.Mechatronics.SystemObjectRelationType

Bases: object

Relation type.

Enum Members

Enum Member Enum Member Description
Ecad
ECAD relation type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.