SpringDamperBuilderAxisJointType Enumeration

NXOpen.Mechatronics.SpringDamperBuilder.AxisJointType is an alias for NXOpen.Mechatronics.SpringDamperBuilderAxisJointType

class NXOpen.Mechatronics.SpringDamperBuilderAxisJointType

Bases: object

the Axis Joint types.

Enum Members

Enum Member Enum Member Description
Angular
Angular
Linear
Linear
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.