SpeedControlBuilder Class¶
-
class
NXOpen.Mechatronics.
SpeedControlBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.SpeedControl
builder.To create a new instance of this class, use
NXOpen.Mechatronics.SpeedControlCollection.CreateSpeedControlBuilder()
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
AxisJoint | Returns the joint select. |
AxisType | Returns or sets the axis joint type. |
DirectionType | Returns or sets the direction type, which works only when the speed control is used to drive NXOpen.Mechatronics.TransportSurface |
EnableLimitForce | Returns or sets whether or not to enable the limit force. |
ForwardForce | Returns the forward force that speed control can apply. |
LimitJerk | Returns or sets the limit jerk flag, which is used to control if the speed control includes jerk data. |
MaxAcceleration | Returns the max acceleration, which is used to set the maximum acceleration for speed control. |
MaxJerk | Returns the max jerk, which is used to set the maximum jerk for speed control. |
Name | Returns or sets the name. |
ReverseForce | Returns the min force that speed control can apply. |
Speed | Returns the speed. |
Tag | Returns the Tag for this object. |
UseAcceleration | Returns or sets the use acceleration flag, which is used to control if the speed control includes acceleration data. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAxisJoint | Sets the joint. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SpeedControlBuilderAxisJointType Enumeration | the Axis Joint types. |
Property Detail¶
AxisJoint¶
-
SpeedControlBuilder.
AxisJoint
¶ Returns the joint select.
This can be a
NXOpen.Mechatronics.HingeJoint
,NXOpen.Mechatronics.SlidingJoint
,NXOpen.Mechatronics.CylindricalJoint
andNXOpen.Mechatronics.TransportSurface
.-------------------------------------
Getter Method
Signature
AxisJoint()
Returns: Return type: NXOpen.Mechatronics.SelectPhysicsJoint
New in version NX7.5.1.
License requirements: None.
AxisType¶
-
SpeedControlBuilder.
AxisType
¶ Returns or sets the axis joint type.
-------------------------------------
Getter Method
Signature
AxisType()
Returns: Return type: NXOpen.Mechatronics.SpeedControlBuilderAxisJointType
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisType(axisType)
Parameters: axisType ( NXOpen.Mechatronics.SpeedControlBuilderAxisJointType
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
DirectionType¶
-
SpeedControlBuilder.
DirectionType
¶ Returns or sets the direction type, which works only when the speed control is used to drive
NXOpen.Mechatronics.TransportSurface
-------------------------------------
Getter Method
Signature
DirectionType()
Returns: Return type: NXOpen.Mechatronics.SpeedPositionControlDirectiontype
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionType(directionType)
Parameters: directionType ( NXOpen.Mechatronics.SpeedPositionControlDirectiontype
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnableLimitForce¶
-
SpeedControlBuilder.
EnableLimitForce
¶ Returns or sets whether or not to enable the limit force.
-------------------------------------
Getter Method
Signature
EnableLimitForce()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableLimitForce(enable)
Parameters: enable (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ForwardForce¶
-
SpeedControlBuilder.
ForwardForce
¶ Returns the forward force that speed control can apply.
-------------------------------------
Getter Method
Signature
ForwardForce()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
LimitJerk¶
-
SpeedControlBuilder.
LimitJerk
¶ Returns or sets the limit jerk flag, which is used to control if the speed control includes jerk data.
-------------------------------------
Getter Method
Signature
LimitJerk()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitJerk(limitJerk)
Parameters: limitJerk (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MaxAcceleration¶
-
SpeedControlBuilder.
MaxAcceleration
¶ Returns the max acceleration, which is used to set the maximum acceleration for speed control.
-------------------------------------
Getter Method
Signature
MaxAcceleration()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
MaxJerk¶
-
SpeedControlBuilder.
MaxJerk
¶ Returns the max jerk, which is used to set the maximum jerk for speed control.
-------------------------------------
Getter Method
Signature
MaxJerk()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReverseForce¶
-
SpeedControlBuilder.
ReverseForce
¶ Returns the min force that speed control can apply.
-------------------------------------
Getter Method
Signature
ReverseForce()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Speed¶
-
SpeedControlBuilder.
Speed
¶ Returns the speed.
-------------------------------------
Getter Method
Signature
Speed()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: None.
UseAcceleration¶
-
SpeedControlBuilder.
UseAcceleration
¶ Returns or sets the use acceleration flag, which is used to control if the speed control includes acceleration data.
-------------------------------------
Getter Method
Signature
UseAcceleration()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseAcceleration(useAcceleration)
Parameters: useAcceleration (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
SetAxisJoint¶
-
SpeedControlBuilder.
SetAxisJoint
¶ Sets the joint.
Signature
SetAxisJoint(axisJoint)
Parameters: axisJoint ( NXOpen.NXObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
SpeedControlBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.