SignalMappingBuilder Class¶
-
class
NXOpen.Mechatronics.
SignalMappingBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.SignalMappingBuilder
To create a new instance of this class, use
NXOpen.Mechatronics.PhysicsManager.CreateSignalMappingBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
MATLABSignalConnectionList | Returns the MATLAB Signal Connection Builder list |
SHMSignalConnectionList | Returns the SHM Signal Connection Builder list |
SignalConnectionList | Returns the signal connection builder list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetFolder |
|
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SignalMappingBuilderAppOption Enumeration | the application option |
Property Detail¶
MATLABSignalConnectionList¶
-
SignalMappingBuilder.
MATLABSignalConnectionList
¶ Returns the MATLAB Signal Connection Builder list
-------------------------------------
Getter Method
Signature
MATLABSignalConnectionList()
Returns: Return type: NXOpen.Mechatronics.MATLABSignalConnectionBuilderList
New in version NX11.0.0.
License requirements: None.
SHMSignalConnectionList¶
-
SignalMappingBuilder.
SHMSignalConnectionList
¶ Returns the SHM Signal Connection Builder list
-------------------------------------
Getter Method
Signature
SHMSignalConnectionList()
Returns: Return type: NXOpen.Mechatronics.SHMSignalConnectionBuilderList
New in version NX9.0.0.
License requirements: None.
SignalConnectionList¶
-
SignalMappingBuilder.
SignalConnectionList
¶ Returns the signal connection builder list
-------------------------------------
Getter Method
Signature
SignalConnectionList()
Returns: Return type: NXOpen.Mechatronics.SignalConnectionBuilderList
New in version NX8.5.0.
License requirements: None.
Method Detail¶
SetFolder¶
-
SignalMappingBuilder.
SetFolder
¶ Sets folder in which the newly created connections will be stored.
Signature
SetFolder(tgFolder)
Parameters: tgFolder ( NXOpen.Mechatronics.PMNavFolderObject
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
SignalMappingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.