SignalAdapterBuilderDataType Enumeration

NXOpen.Mechatronics.SignalAdapterBuilder.DataType is an alias for NXOpen.Mechatronics.SignalAdapterBuilderDataType

class NXOpen.Mechatronics.SignalAdapterBuilderDataType

Bases: object

Represents the data type.

Enum Members

Enum Member Enum Member Description
Bool
bool
Int
int
Double
double
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.