SignalAdapterBuilderDataPortType Enumeration

NXOpen.Mechatronics.SignalAdapterBuilder.DataPortType is an alias for NXOpen.Mechatronics.SignalAdapterBuilderDataPortType

class NXOpen.Mechatronics.SignalAdapterBuilderDataPortType

Bases: object

Represents the data port type.

Enum Members

Enum Member Enum Member Description
Input
Input
Output
Output
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.