ScrewJointCollection Class¶
-
class
NXOpen.Mechatronics.
ScrewJointCollection
¶ Bases:
object
Represents a collection of Screw Joint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateScrewJointBuilder |
|
FindObject | Finds the NXOpen.Mechatronics.ScrewJoint with the given name. An exception will be thrown if no object can be found with given name. |
Method Detail¶
CreateScrewJointBuilder¶
-
ScrewJointCollection.
CreateScrewJointBuilder
¶ Creates a
NXOpen.Mechatronics.ScrewJointBuilder
.Signature
CreateScrewJointBuilder(cylinJoint)
Parameters: cylinJoint ( NXOpen.Mechatronics.ScrewJoint
) –NXOpen.Mechatronics.ScrewJoint
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ScrewJointBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ScrewJointCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ScrewJoint
with the given name. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.ScrewJoint
.Returns: NXOpen.Mechatronics.ScrewJoint
with this name.Return type: NXOpen.Mechatronics.ScrewJoint
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)