SHMSignalConnectionBuilderStreamIOType Enumeration

NXOpen.Mechatronics.SHMSignalConnectionBuilder.StreamIOType is an alias for NXOpen.Mechatronics.SHMSignalConnectionBuilderStreamIOType

class NXOpen.Mechatronics.SHMSignalConnectionBuilderStreamIOType

Bases: object

Represents the mapping data sream direction.

Enum Members

Enum Member Enum Member Description
Tomcd
write to MCD
Toshm
write to SHM
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.