SCOUTExportBuilderExportFileType Enumeration

NXOpen.Mechatronics.SCOUTExportBuilder.ExportFileType is an alias for NXOpen.Mechatronics.SCOUTExportBuilderExportFileType

class NXOpen.Mechatronics.SCOUTExportBuilderExportFileType

Bases: object

Represents the export file type.

Enum Members

Enum Member Enum Member Description
Csv
CSV File
Xml
XML File
Vdi
VDI File
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.