RuntimeNCBuilder Class¶
-
class
NXOpen.Mechatronics.
RuntimeNCBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.RuntimeNCBuilder
.To create a new instance of this class, use
NXOpen.Mechatronics.RuntimeNCCollection.CreateRuntimeNcBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FlagOfUsingContainer | Returns or sets the flag which indicates whether to put the MCD connected objects to the specific ‘Runtime NC’ container or not. |
FlagOfUsingSpecifiedMCF | Returns or sets the flag which indicates whether use the specified MCF or not. |
Name | Returns or sets the name. |
SpecifiedMCF | Returns or sets the user specified MCF File. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ExportNCCode | This method is used to export current loaded NC Code to disk file. |
GetAxesAndMachineEvents | This method is used to get the axes that involved the motion of CSE output event, and the machine event (e. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMCDConnection | This method is used to get the MCD connected object to the specified axis or machine event @return MCD connected object. |
GetObject | Returns the object currently being edited by this builder. |
LoadNCFile | This method is used to load NC file. |
RunCSE | This method is used to run NC Code via CSE in order to get output events |
SetMCDConnection | This method is used to set the MCD connected object to the specified axis or machine event |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateNCCode | This method is used to update NC code. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FlagOfUsingContainer¶
-
RuntimeNCBuilder.
FlagOfUsingContainer
¶ Returns or sets the flag which indicates whether to put the MCD connected objects to the specific ‘Runtime NC’ container or not.
true means put the MCD connected objects to the specific container (creates the container if it is not exist); false means restore the MCD connected objects to the original default folder, and remove the ‘Runtime NC’ container.
-------------------------------------
Getter Method
Signature
FlagOfUsingContainer()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlagOfUsingContainer(flagOfUsingContainer)
Parameters: flagOfUsingContainer (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FlagOfUsingSpecifiedMCF¶
-
RuntimeNCBuilder.
FlagOfUsingSpecifiedMCF
¶ Returns or sets the flag which indicates whether use the specified MCF or not.
True means use user specified MCF file for running CSE, or use the Standard MCF file in MCD kits.
-------------------------------------
Getter Method
Signature
FlagOfUsingSpecifiedMCF()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlagOfUsingSpecifiedMCF(flagOfUsingSpecifiedMCF)
Parameters: flagOfUsingSpecifiedMCF (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Name¶
-
RuntimeNCBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SpecifiedMCF¶
-
RuntimeNCBuilder.
SpecifiedMCF
¶ Returns or sets the user specified MCF File.
-------------------------------------
Getter Method
Signature
SpecifiedMCF()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecifiedMCF(specifiedMCF)
Parameters: specifiedMCF (str) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
ExportNCCode¶
-
RuntimeNCBuilder.
ExportNCCode
¶ This method is used to export current loaded NC Code to disk file.
Signature
ExportNCCode(ncFile)
Parameters: ncFile (str) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetAxesAndMachineEvents¶
-
RuntimeNCBuilder.
GetAxesAndMachineEvents
¶ This method is used to get the axes that involved the motion of CSE output event, and the machine event (e.
g. ToolChange) that fired by CSE. These axes and machine events are used to connect with MCD objects, so in the MCD simulation stage, the CSE will know which MCD runtime object will be driven.
Signature
GetAxesAndMachineEvents()
Returns: a tuple Return type: A tuple consisting of (axisNames, machineEventNames). axisNames is a list of str. The axis names which involved in CSE motion. machineEventNames is a list of str. The name of events fired by CSE. New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetMCDConnection¶
-
RuntimeNCBuilder.
GetMCDConnection
¶ This method is used to get the MCD connected object to the specified axis or machine event
Signature
GetMCDConnection(isAxis, axisOrEventName)
Parameters: - isAxis (bool) – Flag indicates whether the MCD object is set to connect with axis or machine event.
- axisOrEventName (str) – Axis or machine event name.
Returns: MCD connected object.
The object type can be Mechatronics.PositionControl for the motion axis; or Mechatronics.SpeedControl for the spinde axis; or Mechatronics.GanttOperationObject for the machine event. :rtype:
NXOpen.TaggedObject
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LoadNCFile¶
-
RuntimeNCBuilder.
LoadNCFile
¶ This method is used to load NC file.
Signature
LoadNCFile(ncFile)
Parameters: ncFile (str) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RunCSE¶
-
RuntimeNCBuilder.
RunCSE
¶ This method is used to run NC Code via CSE in order to get output events
Signature
RunCSE()
Returns: a tuple Return type: A tuple consisting of (isRunningOK, errMsg, lineNum, ncLine). isRunningOK is a bool. True means CSE returns succeed result, or failure. errMsg is a str. Error message if CSE return false. lineNum is a int. The NC line number at which CSE failed. ncLine is a str. The NC Code for which CSE failed. New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetMCDConnection¶
-
RuntimeNCBuilder.
SetMCDConnection
¶ This method is used to set the MCD connected object to the specified axis or machine event
Signature
SetMCDConnection(isAxis, axisOrEventName, mcdConnectedTag)
Parameters: - isAxis (bool) – Flag indicates whether the MCD object is set to connect with axis or machine event.
- axisOrEventName (str) – Axis or machine event name.
- mcdConnectedTag (
NXOpen.TaggedObject
) – MCD connected object. The object type can be Mechatronics.PositionControl for the motion axis; or Mechatronics.SpeedControl for the spinde axis; or Mechatronics.GanttOperationObject for the machine event.
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpdateNCCode¶
-
RuntimeNCBuilder.
UpdateNCCode
¶ This method is used to update NC code.
Signature
UpdateNCCode(ncCodeLines)
Parameters: ncCodeLines (list of str) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
RuntimeNCBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.