RigidBodyBuilderMassPropertiesOption Enumeration

NXOpen.Mechatronics.RigidBodyBuilder.MassPropertiesOption is an alias for NXOpen.Mechatronics.RigidBodyBuilderMassPropertiesOption

class NXOpen.Mechatronics.RigidBodyBuilderMassPropertiesOption

Bases: object

the mass property option.

Enum Members

Enum Member Enum Member Description
Automatic
automatic
UserDefined
user defined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.