RequirementCollection Class¶
-
class
NXOpen.Mechatronics.
RequirementCollection
¶ Bases:
object
Represents a
NXOpen.Mechatronics.RequirementCollection
To obtain an instance of this class, refer to
NXOpen.Mechatronics.MechatronicsManager
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateRequirementBuilder | Create builder for Requirement class @return NXOpen.Mechatronics.RequirementBuilder object |
FindObject | Finds the NXOpen.Mechatronics.Requirement object with the given name. |
Method Detail¶
CreateRequirementBuilder¶
-
RequirementCollection.
CreateRequirementBuilder
¶ Create builder for Requirement class
Signature
CreateRequirementBuilder(object)
Parameters: object ( NXOpen.Mechatronics.Requirement
) –NXOpen.Mechatronics.Requirement
to be edited, if None then create a new oneReturns: NXOpen.Mechatronics.RequirementBuilder
objectReturn type: NXOpen.Mechatronics.RequirementBuilder
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
RequirementCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.Requirement
object with the given name.Signature
FindObject(name)
Parameters: name (str) – Name of the requirement object, actually it shall be handle. Returns: NXOpen.Mechatronics.Requirement
object with this name.Return type: NXOpen.Mechatronics.Requirement
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)