ProxyObjectBuilderType Enumeration

NXOpen.Mechatronics.ProxyObjectBuilder.Type is an alias for NXOpen.Mechatronics.ProxyObjectBuilderType

class NXOpen.Mechatronics.ProxyObjectBuilderType

Bases: object

the Builder types.

Enum Members

Enum Member Enum Member Description
RuntimeParameters
Runtime Parameters
ProxyObject
Proxy Object
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.