PositionSensorCollection Class¶
-
class
NXOpen.Mechatronics.
PositionSensorCollection
¶ Bases:
object
Represents a collection of Position Sensor.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreatePositionSensorBuilder |
|
FindObject |
|
Method Detail¶
CreatePositionSensorBuilder¶
-
PositionSensorCollection.
CreatePositionSensorBuilder
¶ Creates a
NXOpen.Mechatronics.PositionSensorBuilder
.Signature
CreatePositionSensorBuilder(positionSensor)
Parameters: positionSensor ( NXOpen.Mechatronics.PositionSensor
) –NXOpen.Mechatronics.PositionSensor
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.PositionSensorBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
PositionSensorCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.PositionSensor
with the given name. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.PositionSensor
.Returns: NXOpen.Mechatronics.PositionSensor
with this name.Return type: NXOpen.Mechatronics.PositionSensor
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)