PositionControlBuilderAxis Enumeration

NXOpen.Mechatronics.PositionControlBuilder.Axis is an alias for NXOpen.Mechatronics.PositionControlBuilderAxis

class NXOpen.Mechatronics.PositionControlBuilderAxis

Bases: object

the axis types.

Enum Members

Enum Member Enum Member Description
Angular
angular
Linear
linear
Mixed
Mix angular and linear
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.