ObjectTransformerBuilderTransformSourceType Enumeration

NXOpen.Mechatronics.ObjectTransformerBuilder.TransformSourceType is an alias for NXOpen.Mechatronics.ObjectTransformerBuilderTransformSourceType

class NXOpen.Mechatronics.ObjectTransformerBuilderTransformSourceType

Bases: object

the transform option.

Enum Members

Enum Member Enum Member Description
AnyObject
Any copied objects
OnlySelected
Selected sources
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.