ObjectSourceBuilderCopyEventTriggerOption Enumeration

NXOpen.Mechatronics.ObjectSourceBuilder.CopyEventTriggerOption is an alias for NXOpen.Mechatronics.ObjectSourceBuilderCopyEventTriggerOption

class NXOpen.Mechatronics.ObjectSourceBuilderCopyEventTriggerOption

Bases: object

Trigger Option in copy event.

Enum Members

Enum Member Enum Member Description
TimeBased
TimeBased
OncePerActivation
OncePerActivation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.