ObjectSinkBuilder Class¶
-
class
NXOpen.Mechatronics.
ObjectSinkBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ObjectSink
builder.To create a new instance of this class, use
NXOpen.Mechatronics.ObjectSinkCollection.CreateObjectSinkBuilder()
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
CollisionSensor | Returns the object select. |
DeleteSource | Returns or sets the option to delete source. |
Name | Returns or sets the name. |
Source | Returns the source select. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetCollisionSensor | Sets the collision sensor object. |
SetSource | Sets the source. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ObjectSinkBuilderDeleteSourceType Enumeration | the delete option. |
Property Detail¶
CollisionSensor¶
-
ObjectSinkBuilder.
CollisionSensor
¶ Returns the object select.
This can be a
NXOpen.Mechatronics.CollisionSensor
.-------------------------------------
Getter Method
Signature
CollisionSensor()
Returns: Return type: NXOpen.Mechatronics.SelectCollisionSensorList
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
DeleteSource¶
-
ObjectSinkBuilder.
DeleteSource
¶ Returns or sets the option to delete source.
-------------------------------------
Getter Method
Signature
DeleteSource()
Returns: Return type: NXOpen.Mechatronics.ObjectSinkBuilderDeleteSourceType
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
DeleteSource(deleteSource)
Parameters: deleteSource ( NXOpen.Mechatronics.ObjectSinkBuilderDeleteSourceType
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Name¶
-
ObjectSinkBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Source¶
-
ObjectSinkBuilder.
Source
¶ Returns the source select.
-------------------------------------
Getter Method
Signature
Source()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
SetCollisionSensor¶
-
ObjectSinkBuilder.
SetCollisionSensor
¶ Sets the collision sensor object.
Signature
SetCollisionSensor(objects)
Parameters: objects (list of NXOpen.Mechatronics.CollisionSensor
) – Collision Sensor objectsNew in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetSource¶
-
ObjectSinkBuilder.
SetSource
¶ Sets the source.
Signature
SetSource(objects)
Parameters: objects (list of NXOpen.NXObject
) – Source objectsNew in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ObjectSinkBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.