OPCClientBuilderTagAccess Enumeration¶
NXOpen.Mechatronics.OPCClientBuilder.TagAccess is an alias for NXOpen.Mechatronics.OPCClientBuilderTagAccess
-
class
NXOpen.Mechatronics.
OPCClientBuilderTagAccess
¶ Bases:
object
the access right of OPC item.
Enum Members
Enum Member Enum Member Description ReadOnly read onlyWriteOnly write onlyReadWrite read and write-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-