MotionProfileBuilderProfileCyclicType Enumeration¶
NXOpen.Mechatronics.MotionProfileBuilder.ProfileCyclicType is an alias for NXOpen.Mechatronics.MotionProfileBuilderProfileCyclicType
-
class
NXOpen.Mechatronics.
MotionProfileBuilderProfileCyclicType
¶ Bases:
object
Indicates which cyclic type should be take.
The type of Cam Profile can be switched between non-cyclic, cyclic and relative cyclic.
Enum Members
Enum Member Enum Member Description RelativeCyclic Relative CyclicCyclic CyclicNonCyclic Non-cyclic-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-