MechatronicsSessionSimulationAction Enumeration

NXOpen.Mechatronics.MechatronicsSession.SimulationAction is an alias for NXOpen.Mechatronics.MechatronicsSessionSimulationAction

class NXOpen.Mechatronics.MechatronicsSessionSimulationAction

Bases: object

Represents the action of simulation.

Enum Members

Enum Member Enum Member Description
Start
Start
Restart
Restart
Pause
Pause
Resume
Resume
Stop
Stop
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.