MATLABClientBuilder Class¶
-
class
NXOpen.Mechatronics.
MATLABClientBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.MATLABClientBuilder
To create a new instance of this class, use
NXOpen.Mechatronics.PhysicsManager.CreateMatlabclientBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
MATLABServerProgID | Returns or sets the MATLAB server prog ID. |
MatlabFileBrowser | Returns or sets the simulink file browser. |
Tag | Returns the Tag for this object. |
UpdateTime | Returns the update time. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAvailableItems | Get the available MATLAB items. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetItemAttributes | Get the attribute of MATLAB items |
GetObject | Returns the object currently being edited by this builder. |
SetAvailableItems | Set the available MATLAB items. |
SetItemAttributes | Set the attribute of MATLAB items |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MATLABClientBuilderDataPortType Enumeration | Represents the data port type. |
MATLABClientBuilderDataType Enumeration | Represents the data type. |
Structs¶
MATLABClientBuilderSignalData_Struct Struct | Defines the signal data. |
MATLABClientBuilderTagAttribute_Struct Struct | the attribute of MATLAB item. |
Property Detail¶
MATLABServerProgID¶
-
MATLABClientBuilder.
MATLABServerProgID
¶ Returns or sets the MATLAB server prog ID.
-------------------------------------
Getter Method
Signature
MATLABServerProgID()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MATLABServerProgID(matlabServerProgID)
Parameters: matlabServerProgID (str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MatlabFileBrowser¶
-
MATLABClientBuilder.
MatlabFileBrowser
¶ Returns or sets the simulink file browser.
-------------------------------------
Getter Method
Signature
MatlabFileBrowser()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MatlabFileBrowser(filename)
Parameters: filename (str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpdateTime¶
-
MATLABClientBuilder.
UpdateTime
¶ Returns the update time.
-------------------------------------
Getter Method
Signature
UpdateTime()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Method Detail¶
GetAvailableItems¶
-
MATLABClientBuilder.
GetAvailableItems
¶ Get the available MATLAB items.
Signature
GetAvailableItems()
Returns: a tuple Return type: A tuple consisting of (signalName, signalType). signalName is a list of str. signalType is a list of NXOpen.Mechatronics.MATLABClientBuilderDataType
.New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetItemAttributes¶
-
MATLABClientBuilder.
GetItemAttributes
¶ Get the attribute of MATLAB items
Signature
GetItemAttributes()
Returns: Return type: list of NXOpen.Mechatronics.MATLABClientBuilderTagAttribute_Struct
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetAvailableItems¶
-
MATLABClientBuilder.
SetAvailableItems
¶ Set the available MATLAB items.
Signature
SetAvailableItems(signalName, signalType)
Parameters: - signalName (list of str) –
- signalType (list of
NXOpen.Mechatronics.MATLABClientBuilderDataType
) –
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetItemAttributes¶
-
MATLABClientBuilder.
SetItemAttributes
¶ Set the attribute of MATLAB items
Signature
SetItemAttributes(attr)
Parameters: attr (list of NXOpen.Mechatronics.MATLABClientBuilderTagAttribute_Struct
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
MATLABClientBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.