LogicObjectCollection Class¶
-
class
NXOpen.Mechatronics.
LogicObjectCollection
¶ Bases:
object
Represents a
NXOpen.Mechatronics.LogicObjectCollection
To obtain an instance of this class, refer to
NXOpen.Mechatronics.MechatronicsManager
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateLogicObjectBuilder | Create builder for LogicObject class @return NXOpen.Mechatronics.LogicObjectBuilder object |
FindObject | Finds the NXOpen.Mechatronics.LogicObject object with the given name. |
Method Detail¶
CreateLogicObjectBuilder¶
-
LogicObjectCollection.
CreateLogicObjectBuilder
¶ Create builder for LogicObject class
Signature
CreateLogicObjectBuilder(object)
Parameters: object ( NXOpen.Mechatronics.LogicObject
) –NXOpen.Mechatronics.LogicObject
to be edited, if None then create a new oneReturns: NXOpen.Mechatronics.LogicObjectBuilder
objectReturn type: NXOpen.Mechatronics.LogicObjectBuilder
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
LogicObjectCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.LogicObject
object with the given name.Signature
FindObject(name)
Parameters: name (str) – Name of the Logic object, actually it shall be handle. Returns: NXOpen.Mechatronics.LogicObject
object with this name.Return type: NXOpen.Mechatronics.LogicObject
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)