LimitSwitchCollection Class¶
-
class
NXOpen.Mechatronics.
LimitSwitchCollection
¶ Bases:
object
Represents a collection of Limit Switch.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateLimitSwitchBuilder |
|
FindObject |
|
Method Detail¶
CreateLimitSwitchBuilder¶
-
LimitSwitchCollection.
CreateLimitSwitchBuilder
¶ Creates a
NXOpen.Mechatronics.LimitSwitchBuilder
.Signature
CreateLimitSwitchBuilder(limitSwitch)
Parameters: limitSwitch ( NXOpen.Mechatronics.LimitSwitch
) –NXOpen.Mechatronics.LimitSwitch
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.LimitSwitchBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
LimitSwitchCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.LimitSwitch
with the given name. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.LimitSwitch
.Returns: NXOpen.Mechatronics.LimitSwitch
with this name.Return type: NXOpen.Mechatronics.LimitSwitch
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)