GraphControlBuilderSlaveValueUnit Enumeration

NXOpen.Mechatronics.GraphControlBuilder.SlaveValueUnit is an alias for NXOpen.Mechatronics.GraphControlBuilderSlaveValueUnit

class NXOpen.Mechatronics.GraphControlBuilderSlaveValueUnit

Bases: object

the Slave Unit types.

Enum Members

Enum Member Enum Member Description
LinearPosition
Linear Position
RotaryPosition
Rotary Position
LinearSpeed
Linear Speed
RotarySpeed
Rotary Speed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.