GanttLinkerCollection Class¶
-
class
NXOpen.Mechatronics.
GanttLinkerCollection
¶ Bases:
object
Represents a
NXOpen.Mechatronics.GanttCollection
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateGanttLinkerBuilder | Creates a NXOpen.Mechatronics.GanttLinkerBuilder @return |
FindObject | Finds the NXOpen.Mechatronics.GanttLinker with the given name. |
Method Detail¶
CreateGanttLinkerBuilder¶
-
GanttLinkerCollection.
CreateGanttLinkerBuilder
¶ Creates a
NXOpen.Mechatronics.GanttLinkerBuilder
Signature
CreateGanttLinkerBuilder(other)
Parameters: other ( NXOpen.Mechatronics.GanttLinker
) –Returns: Return type: NXOpen.Mechatronics.GanttLinkerBuilder
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
GanttLinkerCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.GanttLinker
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.GanttLinker
.Returns: NXOpen.Mechatronics.GanttLinker
with this name.Return type: NXOpen.Mechatronics.GanttLinker
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)