FunctionObjectCollection Class¶
-
class
NXOpen.Mechatronics.
FunctionObjectCollection
¶ Bases:
object
Represents a
NXOpen.Mechatronics.FunctionObjectCollection
To obtain an instance of this class, refer to
NXOpen.Mechatronics.MechatronicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateAddComponentBuilder | Creates a NXOpen.Mechatronics.AddComponentBuilder @return |
CreateFunctionObjectBuilder | Create builder for FunctionObject class @return NXOpen.Mechatronics.FunctionObjectBuilder object |
DeleteFunction | Dlete a NXOpen.Mechatronics.FunctionObject object |
FindObject | Finds the NXOpen.Mechatronics.FunctionObject object with the given name. |
RenameFunction | Rename a NXOpen.Mechatronics.FunctionObject object |
Method Detail¶
CreateAddComponentBuilder¶
-
FunctionObjectCollection.
CreateAddComponentBuilder
¶ Creates a
NXOpen.Mechatronics.AddComponentBuilder
Signature
CreateAddComponentBuilder()
Returns: Return type: NXOpen.Mechatronics.AddComponentBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CreateFunctionObjectBuilder¶
-
FunctionObjectCollection.
CreateFunctionObjectBuilder
¶ Create builder for FunctionObject class
Signature
CreateFunctionObjectBuilder(object)
Parameters: object ( NXOpen.Mechatronics.FunctionObject
) –NXOpen.Mechatronics.FunctionObject
to be edited, if None then create a new oneReturns: NXOpen.Mechatronics.FunctionObjectBuilder
objectReturn type: NXOpen.Mechatronics.FunctionObjectBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
DeleteFunction¶
-
FunctionObjectCollection.
DeleteFunction
¶ Dlete a
NXOpen.Mechatronics.FunctionObject
objectSignature
DeleteFunction(functionObject)
Parameters: functionObject ( NXOpen.Mechatronics.FunctionObject
) –NXOpen.Mechatronics.FunctionObject
object with this name.New in version NX7.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
FunctionObjectCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.FunctionObject
object with the given name.Signature
FindObject(name)
Parameters: name (str) – Name of the Function object, actually it shall be handle. Returns: NXOpen.Mechatronics.FunctionObject
object with this name.Return type: NXOpen.Mechatronics.FunctionObject
New in version NX7.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RenameFunction¶
-
FunctionObjectCollection.
RenameFunction
¶ Rename a
NXOpen.Mechatronics.FunctionObject
objectSignature
RenameFunction(newName, functionObject)
Parameters: - newName (str) – New name of the Function object.
- functionObject (
NXOpen.Mechatronics.FunctionObject
) –NXOpen.Mechatronics.FunctionObject
object.
New in version NX7.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)